Hi,
As a result of checking that TPS659037 is not working, it is an internal short circuit of VCC1(C7) and CND_ANA(M13).
The customer will ask if the input voltage of 5 volts is measured during a short circuit.
Is 5V measurement normal on VCC1 pin for VCC1 and GND internal short circuit?
12V to 5V Schematic :
Delete
TPS6590377 Schematic :
Delete