This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25306: The charge current exceeds the set value through the ICHG pin

Part Number: BQ25306

Hi TI Teams,

We set the charge current of BQ25306 to 1A(2-cell Li-lon battery), but the actual measured charging current can reach 4A when the battery voltage is low, which have exceed the maximum charging current supported by BQ25306 (3A). 

The schematic is show as below:

The input voltage is 9.5V and the battery is 2-cell Li-lon. The output current waveform of SW pin is as follows:

1) With the load

2) Without the load

Can you help to analyze the cause of this problem?

Thanks,

Kind Regards