Other Parts Discussed in Thread: TPS65982, TPS65987
Hi there,
as some others have asked before, I also need the project files to customize some settings of the PD-Controller on the TUSB1046EVM.
Thanks in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
as some others have asked before, I also need the project files to customize some settings of the PD-Controller on the TUSB1046EVM.
Thanks in advance!
Hi,
I only have the binary file available for TUSB1046EVM, would this work for you?
Thanks
David
Hi, the chip is already flashed and working, but I need to do some changes to the settings, so I'm afraid it won't help. Sorry, my title is imprecise...
Hi Jeromin,
Thank you for reaching out!
The TPS65982 is NRND (Not Recommended for New Design). I would highly recommend using the TPS65987 in your design. Please let me know if you have additional questions.
Best Regards,
Aya
Hi Aya, yes I already noticed that it's NRND, and I will use the TPS65987 in new designs But for now I have the TUSB1046 eval board which is equipped with the TPS65982, and to continue my test I need at least to know what the current settings for the chip on this board are, because they are not mentioned anywhere. For example, I suspect the settings to actual limit the current to 0.5 A, but I can't say it for sure. So, I either need the project files (which someone at TI has for sure) or a list of the chips settings.
Thanks & regards, Jeromin
Hi Jeromin,
I understand your concern. Unfortunately, we do not have the project files. I am looking into obtaining a list of the chip settings and will get back to you early next week. Thank you for your patience.
Best Regards,
Aya