This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76200: bq76200 as high side driver

Part Number: BQ76200

I am using SIR510DP-T1-RE3 as n channel FET with bq76200. The recommended Gate resistance as per N channel FET datasheet is 1 ohm only.

However, as per Beyond the Simple Application Schematic document, moderate resistance >100 ohm is recommended which is quite high.

 

I just want to confirm use of 500 ohm will cause any issue.

I am just confused with which recommendation I should follow.

Thanks in advance