Hi, we are using UCC21739-Q1 in an inverter driving an IGBT, and during double pulse testing we have noticed that the 2 level turn-off is not working correctly.
CH1=input to driver
CH2=Vge
CH3=Vce
CH4=IC
The first waveform is just before the OC event
The second waveform shows the OC event when the OC pin reaches 0.7V which is 7us into the waveform, the fault pin is also responding correctly, but the gate seems to get stuck high for over 2us. At 9us into the waveform it looks like the driver is doing it's 2 level turn-off all be it at the wrong voltage, but the duration seems to match T2LOFF as per the datasheet.
Any support is appreciated.