This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23630: Ton_min of HSOIC package

Part Number: LMR23630

Hi team,

Are the Ton_min specs of HSOIC and WSON the same?

Best Regards,

  • Hello, being that the die is the same, the electrical performance should be nearly identical. though, the min on time which is effectively the blanking time is dependent on inductor current sense settling time, which can be skewed by package design. I will see if the responsible design engineer can provide a value for it.

  • The target on this specification are the same as the WSON package for the HSOIC device, but it was not characterized for the HSOIC. I cannot be for certain, but that could be to why their is no electrical specification stated.