Hi TI Experts, I am testing a board with two Buck-Boost modules, they are identical circuits using LM5118MHX. They are made to accept +7V to +25V and deliver +24V (1.5A), both. I used Webench in order to generate the schematics and I adjust it with my references, but my issue is they are not correctly working.
On several cards we can see that the last Buck-Boost is working great but the first one isn't and it's not all the time like this, sometimes both don't work. I copy/paste the schematics and the only difference is I add a Diode (D101) on the first module to prevent current inversion, apart from that components are the same. Can you help me please, we are going crazy here.
First schematic and circuit :


Second schematic and circuit :


Thanks
John