This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: I want to improve efficiency

Part Number: LM5118

Hi TI experts...

I have a design with these parameters:

Vin = 11 V - 48 V

Vout = 12 V

Iout = 5 A

f = 100 kHz

This is the circuit

these are my measure data:

I would like to raise my red dots above 70%, what do you recommend me to do?

thank you very much in advance.