Hi Team,
My customer now choose a buck-boost in DVR application, the requirement is 9-36Vin, 12Vout, 2A output current, low Iq, high efficiency at light load.
As first they would like to use LM5118. However, met problem.
When LM5118 operate in low power mode (output current is several mA), the efficiency is too low, which can't keep high efficiency at light load.
May I ask do we have much better recommendation about these requirement with high efficiency at light load?
- 9-36Vin, 12Vout, 2A output current, low Iq, high efficiency at light load.
- Customer said that they need to keep dozens mW at light load...(12Vout*3mA)
Thanks!