I am developing a product with a battery management system and found that I needed an input boost converter to mitigate voltage drop on 5VUSB when batteries are charging.
I made a small test PCB for the TPS61022 and wired it into my project...
At system-idle and slow charging (800mA from the 5V3A USB supply), the boost converter functions as expected.
However, when I increase the battery charge rate to 2A, the TPS61022 fails to short-circuit.
Before writing this post, I've read that some others have also experienced similar failures with this chip. Some caused by the output capacitor being too distant, but I don't think that is a problem in my layout. I've tried adding a 100nF capacitor in parallel with the FB resistor R101 ((1 / ((2 * pi) * 2kHz * 820Kohm)), and I've also tried a datasheet suggestion of adding a pre-load diode from VIN to VOUT. To no avail, the ICs are all burning/shorting.
Might there be someone with experience using this chip who can shed light on this issue?
From the specs, it seems this chip can certainly handle 2-3A at 5Vout, so it seems to be an appropriate component selection for this project.
Many thanks.