Hi Team,
Can you help to provide 48Vin to 5Vout/5A efficiency curve in auto-mode/400KHz condition such like below capture for me ? Thanks!
I have try yo use our webench to simulate it, but the curve result seems shown in force-PWM mode instead of auto-mode. The efficiency in below 0.5A load is much lower than 24V/12V, even I use 24Vin in webench, the result still very lower than the datasheet provided, so I guess Webench can only simulate the force PWM mode.
BR,
Kai