Part Number: BQ24196
Other Parts Discussed in Thread: BQ25303J, , BQ24192, BQ24193, BQ24195L, BQ24192I, BQ24190, BQ25606
I have a question about pulling system power directly from a switching battery charger (not through the battery).
I need Vout=4-5.5V, Vin=12-15V (could vary), and 1 cell 4.2V li-ion battery backup in case Vin is disconnected.
In normal mode (Vin present) it should output 3.5-5.5V directly from it's buck (not through the battery).
I see many bq2xxxx have 3.5-4.35V on either SYS or SW pin. Will pulling (50-400mA) from this, disturb the battery charge sensing (since the SW / SYS pin voltage will drop with the external consumption)? I would hate "ripple" charge/dischage, due to the consumption. I would like the battery to be as disconnected as possible, just waiting for Vin to disappear.
The 12V will be able to supply enough for both charging and consumption, so no load sharing.
I have been looking at these:
bq25303J, bq24195L, bq24193, bq24190 / bq24192 / bq24192I, bq24196.
Standalone is a good safety measure, but I will also enable control it from an MCU + i2c bus and shunt voltage monitor.
Would all be good choices?