Other Parts Discussed in Thread: TPS2375EVM,
I am attempting to use PoE to power my design (board powered by DCDC needing power from PoE) but the PD power shuts down when I connect the power out from the TPS2378EVM-105 to my design (after I allowed the CDB to show setup complete). I have successfully done this with the TPS2375EVM but not with this part (TPS2378EVM-105). With the TPS2375EVM, I can set the class to 0 on that EVM and all runs well. I have noted that for the TPS2378EVM-105, it is only hard set to Class 4. It powers up when I connect it with only 4.7kΩ as the load, like the other TPS2375EVM, but when I connect my design board to it, the output drops to 800mV. I tried Class 4 on the TPS2375EVM to imitate this scenario and the same thing happens.
Theoretically, would I have to load up to 12.95W to have Class 4 work? Are the ranges in this table for load wattage "up to the value" or from "minimum load needed to maximum load allow"? Any help would be greatly appreciated.
Thanks,
Nick