Other Parts Discussed in Thread: CSD87330Q3D, 66AK2G12
Hi support team,
This is a confirmation about VDDctrl parts selection.
I would like to confirm how to calculate the inductor and Rtrip.
What design requirements led to these recommendations?
What values did you use in the above formula?
VOUT = 1V
VIN = 5V?
fSW = 340kHz?
IOUTmax = 2.9A?
KIND = 0.3?
ITRIP = 10μA
RDS(on) = 17mΩ?
The low-side RDS(on) of the recommended FET CSD87330Q3D is about 5mΩ, so the calculations do not match.
Regards,
Dice-K