Other Parts Discussed in Thread: TPS54340B
Please let me confirm two points below about synchronizing to system clock.
①Is below schematic no problem?
Clock source is 3.3V CMOS output (Logic IC), it is not Hi-Z.
Clock source is ON at all the time.
Logic IC's supply voltage is the same as TPS54240's Vin (5V).
②Datasheet for TPS54240 is described 10pF and 4kΩ, but TPS4340B is deleted 4kΩ.
What is the background for delete 4kΩ?
Best regards,
Satoshi