Other Parts Discussed in Thread: TLV62565, TPS62A02
Dear TI experts,
I asked review of schematic 4 months ago ;
Actually my customer did lots of tests so far. and they have a related question.
they tested with a standard ISO-7637-2. I think that you already know this standard, but I attach a pdf document for you.
We found that the worst case of input voltage is "Pulse 1" and "Pulse 5b". Please refer the waveform below.
-> Pulse 1
-> Pulse 5b
As You can see, Pulse1 is the waveform that is very close to Vin recommended input range, and Pulse 5b is very close to Vin absolute maximum rating input range. (please see the spike voltage which can found every 20 seconds)
the important thing is that they tested 5,000 times with this input voltage, but the IC is okay and works well.
But my customer worries that this kind of waveform can slightly damage the IC, and finally not working.
so my final question is ; Is it okay with this kinds of input voltage applied to Vin? or is there any possibility to damage the IC with those input voltage?
Please check this issue. Thanks.
Best regards,
Chase