Hello,
I want to validate that the design for enabling the TPS61235PRWLR will not leak much voltage and will work properly. Going into the Vin pin with a 1M ohm resistor in series with a switch that when it is turned on it will go into the enable pin, otherwise it will go to ground. The image below shows the circuit.