This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: Functionality Clarification

Part Number: BQ24171
Other Parts Discussed in Thread: BQ28Z620, CSD25402Q3A, CSD17313Q2

Hi all,

We are thinking about using bq24171 charger IC in our board where we will implement 3.7V 2850 mAh Li-ion battery.

Please clarify the following doubts regarding bq24171 charger IC. 

1. Required system load Power will be provided directly from adaptor right?

2. If battery voltage becomes 2.75V(Fully discharged battery). Will bq24171 isolate system load from battery?

3. If battery polarity is connected reverse, will bq24171 protects the system load? If not what is the solution?

4. Charger IC alone is enough or Do I need battery monitor, battery protector and fuel gauge. Can you provide one reference design where bq24171 is used with battery monitor, battery protector and fuel gauge.

Regards

Akilarasan