This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24735: Abnormal power on of BQ24735, unable to generate normal level on pins 3 and 4

Part Number: BQ24735


Solution: BQ24735RGRR has occasional abnormal power on problem

Fault symptom:

 This fault is caused by occasional system power failure during normal use of the product. The problem may be resolved by shutting down and restarting, or the system may still not be able to power on when restarted;

 By analyzing the faulty instrument, it was found that the fault was due to the inability of pins 3 and 4 of the BQ24735 chip to generate normal level conduction MOS, resulting in the system being unable to supply power;

 The two instruments that had problems at the beginning of the test were all in the same condition. When the fault occurred, the voltage at pins 3 and 4 of BQ24735 chip was 0; During normal operation, the voltage is 12 and 18V, used to conduct two MOS。

 Design:

Waveform of abnormal power on:

Waveform of abnormal power on:

Tested:

1. I have conducted ABA cross experiments before; Fault with the chip;

2. During testing, the display screen and other loads were not connected; Eliminate the issue of load overload;

3. There is a small probability of recurrence of restart failure phenomenon;

4. After looking at the waveform during power on, it was found that the voltage increased rapidly at the ms level during power on, and the voltage decreased slowly during power off

5. As can be seen from the waveform above, the two pins of the chip that works once cannot generate normal levels. They have been trying, but they have been unable to provide normal levels

At present, we are unable to confirm the cause of the problem. Please seek help to resolve it. Thank you!

  • Hello Jun,

    Can you answer a couple questions:

    Can you measure the voltage on the ACDET Pin when the fault occurs?

    What is the Adapter input Current/Voltage?

    Best Regards,

    Christian.

  • Dear Christian,        

           Thank you very much for your reply!

    The input voltage of the adapter is 12V5A, and the ACDET voltage is 2.6V

    Pls refer to!

    Best Regards

  • Hello Jun, 

    This is a strange occurrence. I have a few more questions:

    Is a battery attached when this fault occurs?

    If there is a battery what is the battery voltage?

    Can you send me the register values when the fault is occurring?

    Can you send a waveform of the  ACOK Pin and VCC Pin when the fault is occurring?

    Best Regards,

    Christian

  • Dear Christian,

    Thank you very much for your reply!

    The battery was not connected when this fault occurred.
    The acok waveform only when there is no fault is as follows:


    1. Acdet

    2. 6v output

    3. Acok

    4. Power supply

    This is the waveform order from top to bottom, not the channel order

    Pls refer to!

    Best Regards

  • Hello Jun,

    Thank you for this Information. However, I need the waveform when there is a fault. I need to know what is happing with these waveforms when there is a fault to narrow down what could be causing this issue.

    Can you also provide the register values when there is a fault.

    Best Regards,

    Christian.