Hi team,
Following from the thread below,
Customer test spec that will need to draw 9A for 1s, and see this voltage drop below 18V(customer spec). but changing inductor into 2.2uH, dynamic performance can be improved, is this any potential risk to have to change on inductor? Or we have other components can be modified? Thank you.
L7201 = 10uH
L7201 = 2.2uH