This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi. Is it possible to connect external 12V power supply at the VOUT pin when VIN=0V and EN=OFF. VIN and External 12V will not be applied simultaneously. I would like to know if there are any concerns.
Best regards.
Hi Bryce,
Thanks for the answer. We are designing a power supply with two inputs for industrial application, one for unregulated 12-24V input, the other is for regulated 12V (external 12V in the above diagram).
Best regards,
Hi Keita,
Thanks for feedback. Understood, so the 12V-24V input to TPS552892 is something like backup power supply? Only when external 12V supply is not valid, then TPS552892 can be enabled; if external 12V is already, then TPS552892 is disabled, right?
Regards,
Bryce