I am experiencing an issue where the TPS25982 load switch would not turn OFF at temperatures around -35 C. My schematic is shown below

The board with the TPS25982 contains data acquisition hardware, so I can monitor the voltage on the output pins through vsns_sw. The output of the load switch (out_sw) is not loaded with anything except for the voltage sense circuitry. vsns_sw is measured directly by an ADC (no pullups or down).
Testing Procedure:
1) Set the EN input (cmd_sw) to toggle ON(3.3V) and OFF(0V) every 5 seconds.
2) Put the board in thermal chamber and set the temperature to -40C
3) Bring the board back to room temperature
Here is what I am observing:

1) When approaching temperatures around -30C, the switch after tuning ON fails to turn OFF.

2) This anomalous behavior still occurs when the board is brought to room temperature.
3) Voltage level of EN pin was confirmed with a multi meter to be correct (switching between 3.3V and 0V every 5 seconds).
4) Voltage of the output pin was also confirmed with multi meter to be 12V.
5) When the device output is loaded in this faulty state, it is able to power the load. (Power is coming from the input voltage)
Is this a known issue with the device and what is the fix for this?