This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122-Q1: boot diode selection

Part Number: LM5122-Q1

Hi Team, 

we'd like to choose below diode as boot diode. Not sure about leakage current since datasheet just mentioned it need to be low. Thanks. 

VF=715mV@1mA855mV@10mA

VBR=100VIR 1uA

VBR=70VTJ=150℃,max50uA

BRs

Given 

  • Hello, 

    Thanks for reaching out. As stated in the datasheet at page 20, section 7.3.9: The leakage current of the boot diode should be always less than the BST charge pump sourcing current. From the EC table at page, the charge pump sourcing current is: 

    Please check the leakage current of the diode against this parameter. Let us know if further support is needed. 

    Kind regards,
    EM