Hi team,
Please help confirm that the chip can be used in the following scenarios
The EN pin of the chip controls the output via PWM as follows:
1.Output effective time 3.2ms, shutdown time 21.5ms
2.Output effective time 3.2ms, shutdown time 40.9ms
More than 50% of the chip's life cycle is in the above scenario. It's even 90 percent of the time in the above scenario.
thanks