Other Parts Discussed in Thread: LM2105, UCC27211A
Hello everyone,
I'm designing a Peltier cell controller circuit, and I'll be using a full H-bridge for this purpose. I will control the gate signals of the MOSFETs with a 200kHz PWM signal. I already have the power circuitry implemented, as shown in the image. For controlling the MOSFET gates, I want to use two TPS28225TDRBRQ1 gate drivers. Will this gate driver be suitable for my application? In the datasheet, I see that the maximum frequency is 2MHz, and it can supply up to 4A of current. However, looking at the electrical characteristics tables, it indicates that it can only supply 2A with VUGATE-PHASE = 2.5V and 4A with VLGATE = 2.5V. Oh, I almost forgot, I was planning to use VDD = 7V, although I would prefer to use a gate driver that can support 12V to control the MOSFET gate.
Regards,
Wálter Paz.