Other Parts Discussed in Thread: LM5109, LM5109B
Hello Team,
I am using the LM5109A Half Bridge Gate Driver in design. I need to calculate the current will souce by this device.
I am doing the current calculation on VDD as well as High side and Low Side control input Pins.
1. ON VDD
As per the datasheet current on VDD which is IDDO is 2.9mA.
But there is bootstrap capacitor connected to this Pin. I want to know how much this Bootstrap capacitor will draw the current from VDD Pin apart from IDDO?
2. High side and Low Side control input Pins
How much current will be drawn by Pins 2(HI) and Pin3(LI) ? Does the current on these two Pins will drawn from VDD Pin?
Also, IC peak Output Current is 1A then how the Input side total current on the VDD, HI and LI Pins will contribute.
Please let me know the answer of the above.