Hi team,
Can VREF_SAMP connect the divided resistors? I saw the pin definition said connected to 0.01uF.
But the sector 7.3.1 gives a formula about VREF_SAMP. Should it be VOC_SAMP's formula?
BR
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can VREF_SAMP connect the divided resistors? I saw the pin definition said connected to 0.01uF.
But the sector 7.3.1 gives a formula about VREF_SAMP. Should it be VOC_SAMP's formula?
BR
Leo
If we want to set 0.75V MPP voltage and the Voc is 0.89V. The correct connection is using a divided resistors from Vin_DC to VOC_SAMP?
Hi Leo,
The voltage divider should be placed at VOC_SAMP biased by VIN_DC, here the reference voltage is sampled. The voltage used for reference is VREF_SAMP, which is why it is used in the formula. This voltage is stored at the VREF_SAMP pin across the connected capacitor.
Best Regards,
Juan Ospina