Hi TI team.
The board I am designing requires as one of its functions conduct power from a battery charger to a Li-Ion battery 10s (42 V max) and/or 13s (54.6 V max) charging at 2A.
I required the following protections:
* Transient voltage protection.
* Short circuit protection.
* Inrush current protection & Inrush current limit.
* Reverse polarity protection.
For the transient voltage protection, I will use a TVS but for rest of the protection to not use a discrete solution the TPS26600 or TPS26601 seems a good option.
My question is, can I use this efuse having that battery as load?
Thanks in advance for the reply.