This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005-Q1: LM76005-Q1

Part Number: LM76005-Q1

Hello ,

We are planning to use LM76005-Q1 BUCK Converter in our design for 24V applications. Please find the parameters details mentioned below

Parameters-

Vin max  =  36V

Vin typ   = 24V

Vout       =  12v

Iout       =  3.5A

When we perform the manual calculations by considering data from the data sheet, Tj values is going high due to high Pd , but with the web design files attached above for the reference we don’t see high Power dissipation with parameters mentioned above,

Below i am attaching both ,

1)Manual Calculations for typical value(24V)

2)Web Design Calculations.

Manual Cal-pd.xlsxWBOperatingValuesDesign32.csv

Query 1->What is the efficiency to be considered for the output current of 3.5A

Query2-What is the thermal resistance value to be considered