This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5166: The output voltage tolerance issue

Part Number: LM5166
Other Parts Discussed in Thread: LM5155, LM5165

Hi,

Please kindly review below schedule diagram that we need the output voltage is 3.3V+/-0.05V, and there are some mass product that the output voltage is 3.36V, it maybe 2% failure rate,

and we use the LM5155 has no this issue(The LM5166 don't add R1104 and the ILIM is floating), thanks.