Other Parts Discussed in Thread: LMR51430, LMQ66430, LMR33630
Hello
Currently I am using following DC-DC:
- LM22676TJE-5.0/NOPB - for 16VDC to 12VDC 3A conversion
- LM22676TJE-5.0/NOPB - for 16VDC to 5VDC 3A conversion
- LM22678TJE-ADJ/NOPB - for 16VDC to 3.3VDC 5A conversion
For proper power up sequence I need to power up first 3.3VDC and after this 5VDC. For this I am using an enable pin of LM22676TJE-5.0/NOPB from 16VDC to 5VDC connected with resistors divider to 3.3VDC.
As these parts are relatively old I am concerned about their longevity.
If I want to use a single part number for all 3 converters what you suggest?
1. To use LM22676TJE-5.0/NOPB also for 16VDC to 3.3VDC 3A conversion (3A is enough and I am not must 5A).
2. Or to use another DC-DC with enable pin with better longevity, availability and etc..? If you suggest this option what part number is a recommended one?
Thank you.
Alex