Other Parts Discussed in Thread: TIDA-050012
Hi,
My team has a charger design based on the TPS65987D. It looks quite familiar to the TIDA-050012 EVM board where GPIOs are controlling the output voltage of the DCDC. If a GPIO is enabled the enable on the DCDC is also pulled high. When inserting a phone (tested with two different devices) for charging, the correct voltage is selected (5V in this case), and the DCDC starts to output 5V. No voltage are on VBUS1/2. However after ~250ms the TPS65987D releases the GPIO and restarts. This makes the DCDC to restart its output. From the logs it seems as the board reports overvoltage on the VBUS (VBUSState_MON_HI (0x90))? But when measuring the voltage it is maximum 5.2V. Why do we get this behavior?
Attaching project file, log file and measurement of output from DCDC.
Best regards,
Simon