Other Parts Discussed in Thread: TPSM63610, TPSM63610E
Hi support team,
Are the differences between TPSM63610x and TLVM13610 only the following?
TPSM63610 | TPSM63610E | TLVM13610 | |
VOUT range | 1~20V | 1~20V | 1~10V |
External clock synchronization | Yes | Yes | No |
Forced PWM | Yes (On/Off switchable) | Yes (On/Off switchable) | No |
Spread Spectrum | Yes (On/Off switchable) | Yes (On/Off switchable) | No |
Extended Temperature Range | No | Yes | No |
Please let me know if there are any other differences.
Regards,
Dice-K