Other Parts Discussed in Thread: LM5122, CD74HC4017
dear
LM5122 with four-phase time must use synchronous clock, if the four-phase power is too high, the cost is high, can use three-phase, any advise?thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear
LM5122 with four-phase time must use synchronous clock, if the four-phase power is too high, the cost is high, can use three-phase, any advise?thanks in advance
dear
thanks brigitte reply
we need to design and 120-degree phase-shifting external signal synchronization, using LTC555 clock output drive frequency to decimal counter show in TIDM960.PDF
CD74HC4017, phase-shifting, the current CD74HC4017 output 001 010 011 100 101 and so on achieve different LM5122 to produce out-of-sync (time difference) work, thus achieving phase difference, and then different phase signal superposition to form the maximum output power? I do not know about the principle,thanks
Hi Raymond,
This is a divide-by 6 circuit using one CD74HC4017.
Best Regards,
Feng Ji
Hi Raymond,
For this divide-by 10 circuit, the phase is 36°.
For divide-by 6 circuit, the phase is 60°.
Best Regards,
Feng Ji