Hello E2E Expert,
We are working on BMS application with low side gate driver to driver back to back connected low side MOSFET.
Since this is battery operated device , Gate driver operating current must be very low.
In this application , Gate driver out put will stay in static stage (no switching , either ON or OFF )
I checked with multiple gate driver (UCC27524, UCC27614, etc) but all has supply current in the range of 0.4mA to 1mA.
Can you please suggest gate driver with very low supply current VDD .
Thanks
Regards
Vasu