This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV: LM3409HV Driver shake problem

Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409

According to LM3409 datasheet, we used standard circuit , our application is input voltage is 12V, the output LED lighting is 6V,  the current  is 1A, the Roff=8K, the Coff=470pF, L=100uH, Rsns=0.2, the  EN pin signal is PWM , this PWM frequency is 1K , the LED can be dimming, but when the current is smaller blew 1mA,  this LED lighting will be shake, please give us some advice how to improve it .