This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51362: TPS51362 LP# setting questions enquiry

Part Number: TPS51362

Hello Team,

Customer is in the process of designing with the TPS51362.

 Regarding  TPS51362, customer has conducted some tests as outlined below.

Could you please help clarify the impact of LP# on the Converter?

Vin = 20V, Vout = 1.8V

- LP# = always LOW, customer see no issues under both light and heavy loads, the output voltage maintains at 1.8V.

- During load pull, if LP# is pulled LOW, it doesn't affect the output voltage (maintains at 1.8V).

- With LP# = LOW and no load, IV5 measures 0.035mV/100mΩ which equals 350uA.

- With LP# = 5V and no load, IV5 measures 0.075mV/100mΩ which equals 750uA.

- Whether LP# = LOW or floating (5V), the output remains unaffected under both steady and transient loads.

 

Thanks for your assistance.

 

Best regards,

 

Scott