i need a Wave forms of Data lines after current detection of TPS2540 ic.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We do not have data line waveform after the BC1.2 detection on D+/D- as we release the ownership of these signal after the detection is finished.
The data hub takes ownership of D+/D- after detection and perform enumeration and data transfer. We only pass through the D+/D- and the waveform will be determined by the DFP and UFP.
Regards
Hii Tommy,
If I use tps2540 evaluation board then can I connect slave at the usb male side and at other output female connector side can I use my mobile phone as a master device?
Could you please suggest me how I charge my phone as well as transfer the data at the same time with USB type C?
Hi,
The EVM does not have data capability unless you have a host connected to the plug (J2). Please note that on the TPS2540EVM only the J3 upper connector have data line connected to J2.
The power source of the EVM can either be J2 or J1.
For more information please refer to the EVM user's guide.
Regards