This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR12020: Re: Inductor Selection from datasheet formula and webench calculation doubt

Part Number: LMR12020


Dear Team,

I am using LMR12020 in my design with below mentioned conditions,

As per datasheet I calculated the inductor value as 38uH

Same way I provided the web bench input as above conditions for circuit,

But I am getting the inductor value as 3.3uH only.

Which one is correct and which inductor value I should implement in my design.

Kindly reply ASAP.

Regards,

Rajesh