Dear Team,
Do we have suitable solution can replace MP5496 as below?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
What are the requirements about the switch nodes / output pins maximum currents and operating voltages ? They cannot all be read from the picture due to resolution and the way it was cropped.
Do you need 4 step down DC/DC converters and 5 LDOs ?
Alternatively, there are the TPS6594-Q1 and TPS6593-Q1(preview) which have 5 step down DC/DC converters and 4 LDOs, as well as the TPS65916 and TPS65917-Q1 which have 5 of each.
Additionally, a multi-device configuration can be made combining two or more devices thanks to multi-PMIC synchronization ability present in some devices.
More information about the specific application would help provide better recommendation, but you can have a look at the datasheets for those devices and assess their suitability.
Best regards,
Florian