Hi,
I am working with LM33488MM/NOPB which is a 2.97V to 40V wide Low side N channel controller for switching regulator. Circuit is exactly same as mentioned in datasheet, but we are unable to get the 5V at 1A. Voltage will drop from 5V to 4.32v at 366mA. I have attached a graph of load testing at 5V, please check and provide the necessary information to resolve this issue.