Other Parts Discussed in Thread: LM5156, LM5022
Hi Team,
Can you please suggest the off-line controller for SPEIC converter. (non-isolated). Can I use LM5022-Q1 for the following requirements
Input voltage: 10V to 80V
Output Voltage: 15V or 24V
Rated power: 150W
If any better controller is available, please suggest.
Please do the needful.
Regards
Umamaheswararo