Dear Specialists,
My customer is considering TPS43060 and has a question.
I would be grateful if you could advise.
---
I have a question about the rating of Rcharge
I understand Rcharge is for limiting the current charging the bootstrap capacitor,
A current of VCC/Rcharge flows when the capacitor is not charged at all. It will be 7.5V/4.7ohm= 1.6A, but it doesn't always flow. It just flows a few times.
When switching is performed, I think that the current does not flow so much because the charge consumed by switching is additionally charged.
The value obtained by multiplying that current by the switching frequency is the current value.
After all, how many watts should Rcharge power rating be?
---
I appreciate your great help in advance.
Best regards,
Shinichi