HI Expert
customer would like to configure LED_SET and PWM_FSET but they doesn't heave suitable resistor value for it so they need series resistor for configuration.
LED_SET: 5.76K(accuracy 1%),customer want: 4.7K(1%)+1K(1%)+49.9(1%)+10(1%).
PWM_FSET: 17.7K(1%)m customer want: 12K(1%)+4.7K(1%)+1K(1%)
Support need:
1. Could you please help to check whether can be used in schematic?
2. for accuracy of resistor, how to understand it? in my understand, only choose the value doesn't meet the previous or next thresholds, that will ok?