Hi expert
could you please help review the schematic of LMR33640, it's used on the STB, the actually output is 12V 2A
the inductor parameter: I sat =10A,I_TEMP=6A, DCR=44mohm.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert
could you please help review the schematic of LMR33640, it's used on the STB, the actually output is 12V 2A
the inductor parameter: I sat =10A,I_TEMP=6A, DCR=44mohm.
Hi Feeney,
I suggest raising your inductor to 8.2uH or 10uH according to equation 5 in the data sheet.
Reduce input capacitance to 2x10uF ceramic and 47uF electrolytic, or you may keep 3x10uF ceramic + 68uF electrolytic. Make sure ESR ~100 mOhms for input dampening.
I'd suggest adding a feedforward capacitor DNP parallel to R_fbt. You can populate it at a later time. Also use the recommended resistor network R_fbt = 100k Ohms and R_fbb = 9.09k Ohms, as it is common practice not to use R > 100k.
Cvcc can be reduced to 6.3-10V rating instead of 50V.
A capacitor at the EN pin may interfere with proper dropout of the device, so would suggest to remove or DNP C7P53
Best,
Ryan