Other Parts Discussed in Thread: BQ34Z100, SN74HC164
At a previous job, we used the BQ34Z100-G1 battery gas gauge as part of a larger system (audio system which can be powered by battery or DC power supply, in which the power supply can also charge the battery). I am refreshing my memory on this ASIC, but am I correct in remembering that the PACK- net would be the same "Ground" as the rest of the PCB (and the BAT- would only go to the battery pack negative terminal, as well as the gas gauge's AGND and GND)?
Also, I remember that the gas gauge would show the LED's full-time when the audio system was on, but they would turn off when the system was turned off--although the battery could be charged if the system were plugged into the wall outlet. In the datasheets, the CE (chip enable) pin was connected to the REGIN pin (and the REGIN would be jumpered to the LED's after I2C programming)... If I control the CE pin with the audio system's power (within the voltage rating of the CE pin), would that be the best way to "turn off" the gas gauge LED's when the audio system was turned off? Is there a better way to turn off the LED's when the audio system is turned off? (I cannot remember what we did at my previous job.)