This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Not sure that the product I'm looking for exist. It should behave like LED driver but after looked through different LED I didn't find a product that meet my requirements:
Does such a product exist ?
Thanks.
Hi Pavel,
Which application do you need for such a LED driver? We have many LED drivers that could satisfy the above requirements, so we need to confirm the following spec:
automotive or non-auto?
What is Vin range? Now I know Vout is about 45V.
Do you need only 1 string? What's the Imax of this LED string?
BR, Gracie
Hi Gracie,
First, thanks for feedback.
Application - open space optical communication, so driver should NOT have PWM control, but should feature control input that switch ON/OFF all LEDs.
Vin: it depends on number of LEDs (non-critical parameter). The number of LEDs can vary from 8 to 12. Given that Vf about 3.3V, for 8 LEDs Vin should be 28 ... 32V, for 12 LEDs - 40 ... 45V.
Concerning strings - perhaps 2 strings, e.g. 2 x 8 LEDs.
Imax - 20 ... 30 mA (depends on LED).
Sincerely
Pavel.
Hi Steven,
Sorry, I misunderstood Gracie's request.
Well, the Vin is supplied by a USB powerbank ... so 5V.
Hi Pavel,
Based on your spec, you may need a boost LED driver to boost from 5V to around 45V at 30mA to drive the LEDs.
However, for the "200kb/sec" spec you mentioned, my understanding is you are going to turn on/off the current output 200k times/sec, which is equivalent to 5us per bit. Is my understanding correct? If so, you may need a current rise / fall time less than 1us to meet your requirement. However, this is usually hard to achieve with a boost LED driver. I would recommend you use a pre-boost to boost up the 5V voltage, then use a buck LED driver with shunt dimming (You can check TPS92641 for the shunt dimming feature I mention here) to control the current, which is the fastest method I can think of.
BR,
Steven
Hi Steven,
Thanks. Yes, your understanding is correct. The device you propose TPS92641 features PWM controller (as well as all other LED driver that I saw until now). For my concept I need LED driver without PWM ... but I guess such device doesn't exist. So I'll boost 5V to some level (e.g. 40V), as you suggest, and then use opamps, MOSFET., etc., i.e. "not-integrated" solution.
Sincerely,
Pavel
Hi Pavel,
For the "LED driver without PWM", do you mean a non-switching-type LED driver like TPS92612?
BR,
Steven
Hi Steven,
Yes. ON/OFF is finction of control signal because it is trasmitting data, so NO any PWM activity during phase ON and OFF.
Sincerely,
Pavel
Hi Pavel,
I am not sure if we are understanding the same thing. For switching-type regulator, the current is always on (but with some ripple) unless you turn off the IC. Here is an article that may give you some ideas on how to achieve your target: Common LED Functions and LED Driver Design Considerations
BR,
Steven
Hi Steven,
Seems I misspoke in my previous post.
Without a detailed review of 2 datasheets (i.e. TPS92641 and TPS 92612) I guess the TPS 92612 seems a better fit for what I'm looking for.
In TPS 92612, the PWM is an external input, which can turn on/off the LED array.
On the other hand, at TPS92641, the term PWM is rather related to an internal 1MHz oscillator where the ON/OFF ratio is controlled in a certain way, but what is essential, there is no input where I could apply the data signal.
So indeed, it is interesting to simulate the TPS 92612 in order to check if it is able to drive a series of diodes with a certain datarate (e.g. 200kb/s). It remains to be seen, is it possible to have TPS model 92612 in order to un a simulation and LTSpice.
Sincerely,
Pavel.
Hi Pavel,
Steven is out of office for a biz trip and will reply to you when he comes back, thanks for your patience.
BR
Patrick
Thanks Patrick!
Hi Pavel,
I am currently out of office. I will reply to you next Monday when I am back to office. Thanks for your understanding.
BR,
Steven
Hi Pavel,
For TPS92641, you can apply the data signal to SDIM pin to use the shunt dimming. The TPS92641 is just an example here to illustrate the shunt dimming feature which can achieve high on/off speed. The output current spec of TPS92641 is over-spec for your requirement.
For TPS92612, I am not sure if its output voltage spec can meet your requirement. Also, I am not sure if the on/off speed of TPS92612 can meet your requirement. If you are interested in it, I will assign this thread to the corresponding engineer to help you.
BR,
Steven
Hi Steven,
Not sure that TPS92641 could fit my concept.
Well ... there is Shunt NFET that redirect current on itself switching OFF the LEDs (BTW when the LEDs are OFF, the current is consummed nevertheless). But when the LEDs are ON, the current flowing through the LEDs manifests "the ripples" (i.e. not constant) ... because whole this stuff at left (i.e. Ron, Con, etc.) continue to charge/discharge the coil, isn't it ?
On the other hand, I noticed this sentence in the TPS92612 datasheet: "It is a simple, yet elegant solution to deliver constant current for a single LED string".
Combining it with a single control input (i.e. PWM) gives me some confidence that this controller is capable of doing the job. Why you aren't sure that it can't meet my requirement ?
Sincerely,
Pavel.
P.S. What about simulating TI controllers in LTSpice ... or the only solution is to install TI version of Spice ?
Hi Pavel,
But when the LEDs are ON, the current flowing through the LEDs manifests "the ripples" (i.e. not constant) ... because whole this stuff at left (i.e. Ron, Con, etc.) continue to charge/discharge the coil, isn't it ?
Alright. I think I got your point. You need a linear LED driver for your application. Am I Correct?
Combining it with a single control input (i.e. PWM) gives me some confidence that this controller is capable of doing the job. Why you aren't sure that it can't meet my requirement ?
If you are interested in TPS92612, I will help assign the corresponding engineer to help you.
P.S. What about simulating TI controllers in LTSpice ... or the only solution is to install TI version of Spice ?
This is another topic that is out of my knowledge range. You can raise a new E2E thread regarding this topic and other engineer will help you.
BR,
Steven
Hi Steven,
Alright. I think I got your point. You need a linear LED driver for your application. Am I Correct?
Yes, I don't know how to qualify the type of driver I'm looking for, but briefly... when it's ON, it must be really ON, ie without ripples, when it's OFF it must be really OFF , that is, there is no current through the LEDs.
For the input voltage range, it can only accept 4.5 V – 40 V (lower than the 45V as you mentioned)
Well... that's not really a bad thing because I'd probably opt for two rows of 8 LEDs in series. Since the Vf of these LEDs is around 3.3V, it might work.
For the on/off speed, please refer to Section 6.6 Timing Requirements from the datasheet.
Frankly, I didn't quite understand the meaning of the values in the table in section 6.6. For example, the minimum value for t(PWM_delay_rising) is declared to be 10us. What does this mean exactly? If I apply PWM with t(PWM_delay_rising) = 1us, what will happen? Will the device explode? Or does it just mean that the internal logic driving the NMOS, the source of which is connected to the OUT pin, has a limited slew rate?
This is another topic that is out of my knowledge range.
Ok, can you just confirm that the macromodel of TPS92612 is fairly faithful and I can trust simulations?
If you are interested in TPS92612, I will help assign the corresponding engineer to help you.
Yes, please.
Sincerely,
Pavel.
Indeed, TPS92612 doesn't match speed requirements.
I've simulated the usecase with PSpice for TI and found that maximum clock at PWM about 10kHz (at 20 kHz it's already quite bad)
Hi Pavel,
The t(PWM_delay_rising) and t(PWM_delay_falling) in Section 6.6 Timing Requirements from the TPS92612 datasheet will introduce some delay in your signal input. The t3-t2 and t6-t5 in Figure 1. Output Timing Diagram from the TPS92612 datasheet will limit the maximum on/off speed you can achieve.
I have confirmed with the corresponding engineer who supports TPS92612 that TPS92612 cannot support 200kHz on/off speed.
For such application, I still recommend you use the shunt dimming to achieve this, which is the fastest method I know. You can refer to Figure 16. 100 kHz 50% External FET PWM Dimming VO = 42 V (12 LEDs); VIN = 48 V from LM3409 datasheet to check how fast shunt dimming can do.
BR,
Steven
You can refer to Figure 16. 100 kHz 50% External FET PWM Dimming VO = 42 V (12 LEDs); VIN = 48 V from LM3409 datasheet to check how fast shunt dimming can do.
Hi Steven,
Thanks.
But as can be seen in Fig. 16, when the LED is ON, the current has fairly large ripples that invalidate this device for my app.
Are there any LED drivers that avoid this shortcoming ?
Sincerely,
Pavel
Hi Pavel,
But as can be seen in Fig. 16, when the LED is ON, the current has fairly large ripples that invalidate this device for my app.
There are methods to make the ripple as small as possible, such as enlarging the switching frequency or enlarging the inductor value.
Are there any LED drivers that avoid this shortcoming ?
Sorry. The shunt dimming is currently the only method I know that can fit your 200kb/sec requirement.
BR,
Steven
Hi Steven,
Ok, perhaps by tuning this stuff we can reduce ripples, but classical method (without LED driver) avoids completely this drawback ... like this one:
Here is what this gives:
Well it's less integrated then when using driver (need to add boost converter) ... but finally it does what I want.
Sincerely,
Pavel.
Hi Pavel,
Got it. Thanks for sharing this info. Please let me know if any further support is needed.
Best Regards,
Steven