If two LEDs are connected in series, should the V(OUTx) value be set to the sum of the two forward voltages?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If two LEDs are connected in series, should the V(OUTx) value be set to the sum of the two forward voltages?
Hello Eiji,
Correct, the device will regulate output voltage such that it matches forward voltages. It is important to note that the inputs provided to the device are not voltage based, but current based. By using Rsns and a known Vref the user can set the desired output current and the device will regulate to that current.
Best,
Pedro Arango Ramirez.