Other Parts Discussed in Thread: BQ25970, BQ2597
Hi
I have some questions about the feature of SYNCOUT:
- What is the benefit of SYNCOUT except reducing output voltage ripple?
- Does the phase difference be held 90° by SYNCOUT between master BQ25970 and slave BQ25970?

- We have tested the output voltage of two BQ25970 work parallelly (one is master and the other one is standalone). We found the output voltage ripple is smallest when the phase difference between master BQ25970 and standalone BQ2597 near 180°, and the output voltage ripple is largest when the phase difference between master BQ25970 and standalone BQ2597 near 0°. What causes this phenomenon? And why don't set the phase difference be held 90° by SYNCOUT between master BQ25970 and slave BQ25970?


Thank you very much.
Best regards,
Ryker