This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: EMI

Part Number: LP8866-Q1

Hi Expert:

I have two questions regarding the LP8866-Q1 SNVA964 Application note.

The first question is whether the Figure 7 (b) on page 5 depicts the spread spectrum disabled or spread spectrum enabled with ±3.3% variation?

The second question is, why in (b), the switch frequency harmonics measured values for peak and average at 1.2MHz are the same?

Typically, even with spread spectrum disabled, the average value should be lower than the peak value. Do you have the raw data for this?

Thank you.